DOCA0256EN-01

Interlock Protection Trip Status

The table lists the interlock protection trip status data for the PROFIBUS DP communication.

Slot Index

Byte offset

Size (in bytes)

Byte.Bit

RW

Type

Svd

Parameter name

1 33

48

1

48.0

R

BOOL

N

Interlock 1 trip

48.1

R

BOOL

N

Interlock 2 trip

48.2

R

BOOL

N

Interlock 3 trip

48.3

R

BOOL

N

Interlock 4 trip

48.4

R

BOOL

N

Interlock 5 trip

48.5

R

BOOL

N

Interlock 6 trip

48.6

R

BOOL

N

Interlock 7 trip

48.7

R

BOOL

N

Interlock 8 trip

1 33 49 1

49.0

R

BOOL

N

Interlock 9 trip

49.1

R

BOOL

N

Interlock 10 trip

49.2

R

BOOL

N

Interlock 11 trip

49.3

R

BOOL

N

Interlock 12 trip

49.4–49.7

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?