DOCA0256EN-01

Anti-Backspin Timer Protection

The table lists the anti-backspin timer protection data for the PROFIBUS DP communication.

Slot Index

Byte offset

Size (in bytes)

RW

X

Unit

Type

Range

Default value

Svd

Parameter name

1 7

104

2

RW

1

UINT16

  • 0: Disable

  • 1: Enable

0

Y

Function setting

1 7

106

2

RW

1

s

UINT16

0–60000
(step 1)

0

Y

Time delay

1 7

108

4

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?