Communication Status
The table lists the communication status data for the PROFIBUS DP communication.
| Slot | Index |
Byte offset |
Size (in bytes) |
Byte.Bit |
RW |
Type |
Svd |
Parameter name |
|---|---|---|---|---|---|---|---|---|
| 1 | 33 |
84 |
1 |
84.0 |
R |
BOOL |
N |
PROFIBUS DP port – No communication @Updated D3
|
|
84.1 |
R |
BOOL |
N |
HMI port – No communication |
||||
|
84.2–84.7 |
– |
– |
– |
Reserved |
||||
| 1 | 33 |
85 |
1 |
85.0–85.7 |
– |
– |
– |
Reserved |
| 1 | 33 |
86 |
1 |
86.0–86.7 |
– |
– |
– |
Reserved |
| 1 | 33 |
87 |
1 |
87.0–87.7 |
– |
– |
– |
Reserved |