Motor Data
The table lists the motor data for the PROFIBUS DP communication.
|
Slot |
Index |
Byte offset |
Size (in bytes) |
RW |
X |
Unit |
Type |
Svd |
Parameter name |
|---|---|---|---|---|---|---|---|---|---|
| 1 | 3 |
114 |
2 |
R |
1 |
– |
UINT16 |
N |
Motor status
|
| 1 | 3 |
116 |
2 |
R |
1 |
% |
UINT16 |
Y |
Thermal memory |
| 1 | 3 |
118 |
4 |
R |
1 |
s |
UINT32 |
N |
Thermal time to trip |
| 1 | 3 |
122 |
4 |
R |
1 |
s |
UINT32 |
N |
Thermal time to cool |
| 1 | 3 |
126 |
2 |
R |
1 |
– |
UINT16 |
Y |
Max starts counter or Max starts per hour counter |
| 1 | 3 |
128 |
4 |
R |
1 |
s |
UINT32 |
Y |
Max start time or Max start inhibit time |
| 1 | 3 |
132 |
4 |
R |
0.001 |
A |
UINT32 |
N |
Motor starting peak current |
| 1 | 3 |
136 |
4 |
R |
0.001 |
s |
UINT32 |
N |
Motor starting time |
| 1 | 3 |
140 |
4 |
R |
1 |
min |
UINT32 |
Y |
Total run hour |
| 1 | 3 |
144 |
4 |
R |
1 |
min |
UINT32 |
Y |
Last run hour |
| 1 | 3 |
148 |
2 |
R |
1 |
– |
UINT16 |
Y |
Number of starts |
| 1 | 3 |
150 |
2 |
R |
1 |
– |
UINT16 |
Y |
Number of stops |
| 1 | 3 |
152 |
2 |
R |
1 |
– |
UINT16 |
Y |
Motor stop cause
|
| 1 | 3 |
154 |
2 |
R |
1 |
– |
UINT16 |
Y |
Trip counter |