PROFIBUS DP Settings
The table lists the PROFIBUS DP settings for the PROFIBUS DP communication.
| Slot | Index |
Byte offset |
Size (in bytes) |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Parameter name |
|---|---|---|---|---|---|---|---|---|---|---|---|
| 1 | 9 |
60 |
2 |
RW |
1 |
– |
UINT16 |
2–126 (step 1) |
126 |
Y |
Node address |
| 1 | 9 |
62 |
2 |
RW |
1 |
– |
UINT16 |
0–1 (step 1) |
0 |
Y |
Endian |
| 1 | 9 |
64 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Product profile |
| 1 | 9 |
66 |
6 | – | – | – | – | – | – | – |
Reserved |