DOCA0256EN-01

Reserved

Slot Index Byte offset

Size (in bytes)

Byte.Bit

RW

Type

Svd

Parameter name

1 33 10–11 1

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?