DOCA0256EN-01

Block Output

The table lists the block output data for the PROFIBUS DP communication.

Slot Index

Byte offset

Size (in bytes)

RW

X

Unit

Type

Range

Default value

Svd

Parameter name

1 7

96

2

RW

1

UINT16

  • 0: Disable

  • 1: Enable

0

Y

Function setting

1 7

98

2

RW

0.01

s

UINT16

0–60000
(step 1)

0

Y

Contactor or Breaker open time

1 7

100

4

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?