DOCA0256EN-01

HMI Settings

The table lists the HMI settings for the PROFIBUS DP communication.

Slot Index

Byte offset

Size (in bytes)

RW

X

Unit

Type

Range

Default value

Svd

Parameter name

1 9

48

2

RW

1

UINT16

1–247
(step 1)

1

Y

Node address

1 9

50

2

RW

1

UINT16

0: None

1: Odd

2: Even

2

Y

Parity

1 9

52

2

RW

1

bps

UINT16

0: 2400

1: 4800

2: 9600

3: 19200

4: 38400

5: 57600

6: 115200

3

Y

Baud rate

1 9

54

2

RW

1

UINT16

0: Default

1: Programmable

0

Y

Control keys

1 9 56 2

RW

1

s

UINT16

1–60000
(step 1)
1

Y

Timeout
1 9 58 2

RW

1

BITMAP

Bit 0:

  • 0: Big-endian

  • 1: Little-endian

0

Y

Byte format

NOTE: If LTMTCUF control operator unit is connected on HMI port, HMI port must be configured as follows:
  • Node address: 1

  • Baud rate: 19200 bps

  • Parity: Even

  • Endianness: Big-endian

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?