DOCA0256EN-01

Overview

The table list the different I&M headers. To read I&M data from the device, write the I&M header atleast once after the device is power ON.

Slot Index

Size (in bytes)

Data I&M number
0 255 4

0x08,0x00,0xFD,0xE8

I&M0
0 255 4

0x08,0x00,0xFD,0xE8

I&M1
0 255 4

0x08,0x00,0xFD,0xE8

I&M2
0 255 4

0x08,0x00,0xFD,0xE8

I&M3
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?