DOCA0256EN-01

PKW OUT Data

PKW OUT data request (PROFIBUS DP client to LTMT main unit) is mapped in modules supporting PKW.

To access a register, you must select one of the following function codes:

  • R_REG_16 = 0x25 to read 1 register

  • R_REG_32 = 0x26 to read 2 registers

  • W_REG_16 = 0x2A to write 1 register

  • W_REG_32 = 0x2B to write 2 registers

Word 1

Word 2

Word 3

Word 4

Register address

Toggle bit (bit 15)

Function bits (bits 8 to 14)

Not used

(bits 0 to 7)

Data to write

Register number

0/1

R_REG_16

Code 0x25

0x00

R_REG_32

Code 0x26

W_REG_16

Code 0x2A

Data to write in register

W_REG_32

Code 0x2B

Data to write in register 1 Data to write in register 2

Depending on the PLC platform used, refer to the PKW OUT description in little and big endian formats to know the positioning of each field inside each word.

Any changes in the function field will trigger the handling of the request (except if function code is 0x00).

Toggle bit must change at each consecutive request. This mechanism allows the request initiator to detect that a response is ready by polling the toggle bit in response. When this bit in the OUT data becomes equal to the response emitted toggle bit in the IN data, then the response is ready.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?