DOCA0256EN-01

Phase Over Voltage Protection

The table lists the phase under voltage protection data for the PROFIBUS DP communication.

Slot Index

Byte offset

Size (in bytes)

RW

X

Unit

Type

Range

Default value

Svd

Parameter name

1 6

16

2

RW

1

UINT16

  • 0 - Disable

  • 1 - Alarm
  • 2 - Trip
  • 3 - Alarm and Trip

2

Y

Function setting

1 6

18

2

RW

1

%Vn

UINT16

101–130
(step 1)

110

Y

Pickup

1 6

20

2

RW

0.1

s

UINT16

1–60000
(step 1)

50

Y

Time delay

1 6

22

2

RW

1

%Vn

UINT16

101–130
(step 1)

110

Y

Alarm level

1 6

24

2

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI

  • Bit 2: Communication

  • Bit 3: Auto

3

Y

Reset mode

1 6

26

2

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

1 6

28

2

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?