DOCA0256EN-01

Read Acyclic Data

With DS_Read function, the PROFIBUS DP client can read data from the server.

For example: To read the current protection setting, set the data as follows:

Byte Value
0 (Function number) 0X5E (DS_Read function)
1 (Slot number) 1
2 (Index) 5
3 (Length) 26
4 to 7 Value of the current protection setting

For more information, refer to Data Mapping.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?