260410_LSS900100_eConfigure_KNX_SW

IHC Integration

eConfigure KNX provides full support for IHC (Intelligent House Control) wired systems. You can configure and maintain IHC installations using the IHC Interface and the Wiser for KNX Controller after replacing the original IHC controller.

IHC functionality is available exclusively when the Danish product catalog is selected.

Remote programming, diagnostics, and controller access are supported for IHC installations through the same mechanisms used for KNX.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?