Modbus Registers Tables
Presentation
The Modbus registers of EcoStruxure Panel Server and the Modbus registers of the supported wireless devices connected to it provide measurement and monitoring information.
For detailed information about these Modbus registers, refer to DOCA0241EN EcoStruxure Panel Server - Modbus File.
Table of Modbus Functions
The following table describes the functions supported by the Panel Server to read and/or write data on the Modbus registers of wireless devices.
|
Function code |
Function name |
|---|---|
|
03 |
Read n words |
|
16 |
Write n words |
|
100-4 |
Read n non-adjacent words where n ≤ 100 (refer to Function 100-4: Read Non-Adjacent Registers) |