Analog Module Data
The table lists the analog module data for the PROFIBUS DP communication.
|
Slot |
Index |
Byte offset |
Size (in bytes) |
RW |
X |
Unit |
Type |
Svd |
Parameter name |
|---|---|---|---|---|---|---|---|---|---|
| 1 | 3 |
170 |
2 |
R |
0.1 |
mA |
INT16 |
N |
Analog input 1 |
| 1 | 3 |
172 |
2 |
R |
0.1 |
mA |
INT16 |
N |
Analog input 2 |
| 1 | 3 |
174 |
2 |
R |
0.1 |
mA |
INT16 |
N |
Analog input 3 |
| 1 | 3 |
176 |
2 |
R |
0.1 |
mA |
INT16 |
N |
Analog input 4 |
| 1 | 3 |
178 |
8 |
– |
– |
– |
– |
– |
Reserved |
| 1 | 3 |
186 |
2 |
R |
0.1 |
mA |
INT16 |
N |
Analog output 1 |
| 1 | 3 |
188 |
2 |
R |
0.1 |
mA |
INT16 |
N |
Analog output 2 |
| 1 | 3 | 190 | 4 |
– |
– |
– |
– |
– |
Reserved |