AbandonedGasPipe
The AbandonedGasPipe feature represents gas pipe that have been abandoned in place or used as a conduit; it may also contain selected attributes of GasPipe.
Subtypes: None
Associations: None
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Comments |
text |
User and designer comments. |
|
ConduitIndicator |
text |
Represents pipe that can act as casing for a new pipe; domain values include Yes and No. |
|
ConduitLength |
text |
Length of conduit. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
InstallationDate |
text |
Date of installation. |
|
PropertyUnitCode |
text |
Value assigned to assets to track and classify property records. |
|
Reason |
text |
Code indicating reason for casing; domain values include Highway, Railroad, and Street. |
|
RetiredDate |
date |
The date the device was identified as abandoned. |