Responder Field Model Names
|
Model Name |
Object |
|---|---|
|
RXDEVICEID |
This optional model name is assigned to the RxDeviceID field on the RxLineDisplay feature class. This field holds the ID of the outage device that is causing the de-energized or abnormally energized feeder. This is used by the display de-energized feeders functionality. |
|
RXFEEDERID |
This optional model name is assigned to the RxFeederID field on the RxLineDisplay feature class. This field holds the ID of the feeder that is de-energized. This is used by the display de-energized feeders functionality. |
|
RXINCIDENTID |
This optional model name is assigned to the RxIncidentID field on the RxLineDisplay feature class. This field holds the ID of the incident assigned to the outage. This is used by the display de-energized feeders functionality. |
|
RXPHASE |
This optional model name is assigned to the RxPhase field on the RxLineDisplay feature class. This field holds the Phase value of the feature in the outage. This is used by the display de-energized feeders functionality. |
|
RXREGIONNAME |
This optional field model name is assigned to the Name field on the polygon feature class that represents regions in the geodatabase. Use this field model name only if you wish to configure the Regions functionality. |