Load Summary
Demand from the customer is the load at receiving terminals averaged over a specific time. Demand is expressed in real power, apparent power, or current—kilowatts, reactive volt-amperes, volt-amperes, or amperes.
Associations: None
Subtypes: None
Model Names: LOADSUMMARY
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
CurrentTotal |
long integer |
Amount of current in LoadSummary. |
|
kVAR |
long integer |
Reactance in reactive volt-amperes. |
|
kW |
long integer |
Load summary in kW. |
|
Voltage |
long integer |
Voltage. |