Electric Location
Associations: FacilityStructure, UndergroundStructure
Subtypes: None
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Comments |
text |
User or designer comments. |
|
ConstructionStatus |
long integer |
This field contains a value from the Construction Status domain that indicates the current status of construction on the structure (e.g., proposed, existing, retired). |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
ElectricTraceWeight |
long integer |
Used by Feeder Manager to determine device status and other information that affects circuit connectivity. |
|
FeederID |
text |
Feeder Manager identifier assigned to feeders and devices that participate in a specific distribution circuit. |
|
FeederID2 |
text |
Feeder Manager identifier assigned if device is supplied by second feeder. |
|
FeederInfo |
long integer |
Feeder Manager-assigned phase information describing the phase of the circuit that supplies a device. |
|
InstallationDate |
date |
Date of installation of ElectricLocation. |
|
LocationID |
text |
Utility-assigned identifier of ElectricLocation. |
|
Subtype |
long integer |
Code indicating subtype. |
|
SymbolRotation |
double |
Angle of rotation dictating how a feature appears on the map. |
|
WorkOrderID |
text |
Work order identifier. |