Facility Structure
FacilityStructure is an abstract class containing common attributes of the EquipmentEnclosure abstract class and the SupportStructure feature class (Hframes, poles, towers). EquipmentEnclosure includes these feature classes (and subtypes): SurfaceStructure (pads, pedestals, connection boxes), ElectricStation (main, net, substations), and SwitchingFacility (junction cabinets, switchboards).
FacilityStructure inherits attributes from the Structure abstract class.
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Alternate[X,Y,Z] |
double |
Stores the X, Y, and Z values from a GPS device. |
|
AlternateSource |
text |
This field contains a value from the Feature Source domain that indicates an alternate source for the structure. |
|
FacilityID |
text |
Meaningful company-assigned unique identifier. Many ArcFM tools use the FACILITYID model name on this field. |
|
Owner |
text |
Code indicating owner of structure. Domain values include: Customer Owned, Local Bell, Power Company, Other Utility. |
|
Subtype |
long integer |
Code indicating the type of structure. |
|
SymbolRotation |
double |
Angle of rotation indicating how a feature appears on the map. Uses the SYMBOLROTATION model name. The ArcFM Manual Angle Setter edit task and ArcFM Auto Angle Setter autoupdater both use this field to rotate point features |