LeakReport
Leak reports represent areas on pipes where leaks have been detected. A Leak Report can be associated with any applicable</p>e gas facility (e.g., valves or fittings).
LEAKREPORT is used for gas model configuration. LOCATABLEOBJECT is used to enable the Object Query Locator tool.
Subtypes: None
Associations: GasPipe, LeakRepair
Model Names: LEAKREPORT
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Address |
text |
Address location of reported leak. |
|
ClosedDate |
date |
Date leak report closed. |
|
ClosedStatus |
text |
Code indicating leak closed status; domain values include Active, Cleared, and Repaired. |
|
Comments |
text |
User and designer comments. |
|
CurrentLeakClass |
text |
Code indicating current leak class; domain values include Class 1, Class 2, etc. |
|
DateReported |
date |
Date leak was reported. |
|
DistributionMainObjectID |
long integer |
ObjectID of associated DistributionMain. |
|
DOTReportedIndicator |
text |
Indicates whether leak is reported to DOT; domain values are Yes and No. |
|
FederalLandIndicator |
text |
Indicates whether leak is located on federal land; domain values are Yes and No. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
InstallationDate |
date |
Date of installation. |
|
LastCheckDate |
date |
Date of last leak check. |
|
LeakID |
text |
Utility-defined identifier of leak. Assign the LOCATABLE field model name to enable fields for the Object Query Locator tool. The feature or object class must have the model name LOCATABLEOBJECT assigned. |
|
LeakSurveyType |
text |
Type of survey program used to detect leak; domain values include Aerial, Mobile Truck, and Walking. |
|
NextCheckDate |
date |
Date of next check. |
|
OriginalLeakClass |
text |
Code indicating original leak classification; domain values include Class 1, Class 2, etc. |
|
ServiceObjectID |
long integer |
ObjectID of associated service pipe. |
|
SoilType |
text |
Type of soil in which pipe is buried; domain values include Clay, Rock, Sand, Other, and Unknown. |
|
SurfaceType |
text |
Code indicating ground surface type; domain values include Concrete, Grass, Gravel, Other, and Unknown. |
|
SymbolRotation |
double |
Angle that dictates how the feature appears on map. |