LineHeater
This device is used to heat natural gas inside a pipeline.
Subtypes: None
Associations: None
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Comments |
text |
User or designer comments. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
InstallationDate |
date |
Date of installation. |
|
Owner |
text |
Owner of LineHeater. |
|
PropertyUnitCode |
text |
Value assigned to assets to track and classify Property Records. |
|
SymbolRotation |
double |
Angle that dictates how the feature appears on the map. |