Control Point
ControlPoint can be used to identify specific point depths along a main.
Subtypes: None
Associations: None
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Comments |
text |
User or designer comments. |
|
Depth |
double |
Depth of ControlPoint. |
|
InstallationDate |
date |
Date of installation. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
LocationDescription |
text |
Verbal description of location. |