ValveInspection
This is the inspection of gas valves.
Subtypes: None
Associations: GasValve
Model Names: INSPECTION
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Comments |
text |
User or designer comments. |
|
GasValveObjectID |
long integer |
Object ID of associated gas valve. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
InspectionDate |
date |
Date of last inspection. |
|
Inspector |
text |
Name of inspector during last inspection. |