GasPipeCasing
Gas pipe casing is a conduit through which a gas pipe may be placed. Casings provide gas pipes with protection from undue stress or abrasion.
Subtypes: None
Associations: GasPipe
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
CasingDiameter |
long integer |
Code indicating size of GasPipeCasing; domain values include 2”, 8”, 30”, etc. |
|
CoatingType |
text |
Code indicating type of GasPipeCasing coating; domain values include Bare, Coal Tar Enamel, Paint, etc. |
|
Comments |
text |
User or designer comments. |
|
EndConnection |
text |
Code indicating type of End Connection; domain values include Boot, Homemade, Link Seals, etc. |
|
FillDate |
date |
Date GasPipeCasing was filled. |
|
FillType |
text |
Type of material used for fill; domain values include Dielectric Fluid Filled and Not Filled. |
|
GallonsOfFill |
long integer |
Quantity of filled used, in gallons. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
InServiceDate |
date |
Date pipe set in service. |
|
InstallationDate |
date |
Date of installation. |
|
LengthSource |
text |
Method used to determine length of GasPipe; domain values include FieldMeasurement, Mapping System, and User-Derived. |
|
LocationDescription |
text |
Verbal description of location of GasPipeCasing. |
|
Material |
text |
Material of GasPipeCasing. |
|
MeasuredLength |
double |
Method used to determine length of GasPipe; domain values include FieldMeasurement, Mapping System, and User-Derived. |
|
PropertyUnitCode |
text |
Value assigned to assets to track and classify Property Records. |
|
ProtectionType |
text |
Code indicating type of cathodic protection employed; domain values include Anode, None, and Rectified. |
|
Reason |
text |
Code indicating reason for casing; domain values include Highway, Railroad, and Street. |
|
VentedIndicator |
text |
Indicates presence of ventilator; domain values are Yes and No. |
|
WorkOrderID |
text |
Utility-defined identifier of work order. |