RegulatorStation
A regulator station defines the location of one or more pressure regulators.
The INSETFRAMEOBJECT model name is used in configuring ArcFM Inset Frames. The REGULATOR model name is used for gas tracing functions.
RegulatorStation inherits properties from GasStation and GasDevice abstract classes.
Subtypes: None
Associations: None
Model Names: REGULATOR
Attributes:
|
Field Name |
Field Type |
Description |
|
EmerIsolationSysObjectID |
long integer |
ObjectID of Emergency IsolationSystem of RegulatorStation. |
|
GasPressureSystemObjectID |
long integer |
ObjectID of GasPressureSystem of RegulatorStation. If GASPRESSURESYSTEMSTATUS exists, this field value will be used to specify if the device is a gas pressure system boundary. |
|
GasSystemObjectID |
long integer |
ObjectID of GasSystem of RegulatorStation. |