Odorizer
Because natural gas is odorless and colorless, odorizers are used for leak detection at or near the gas point of purchase. Odorizer delivery methods are based on the size of the system, flow, and electrical power available.
Assign the LOCATABLEOBJECT model name to enable fields for the Object Query Locator tool.
Subtypes: Bypass, Injection Pump, Pulse, RuralTap, Wick
Associations: RuralTap
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Comments |
text |
User or designer comments. |
|
GasTraceWeight |
long integer |
Information used for tracing analysis; stored in a bitgate. Gas Tracing uses the GASTRACEWEIGHT model name. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
InstallationDate |
date |
Date of installation. |
|
Manufacturer |
text |
Manufacturer of Odorizer; domain values include King Tool, Williams Pump, YZ Industries, etc. |
|
Owner |
text |
Owner of Odorizer. |
|
PropertyUnitCode |
text |
Value assigned to assets to track and classify Property Records. |
|
RuralTapObjectID |
long integer |
Object ID of associated RuralTap. |
|
SerialNumber |
text |
Serial Number of Odorizer. Assign the LOCATABLEFIELD model name to enable fields for the Object Query Locator tool. The feature or object class must have the model name LOCATABLEOBJECT assigned. |
|
StorageCapacity |
text |
Amount Odorizer is able to store; domain values include 250#, above ground, .1cc, unknown, etc. |
|
SymbolRotation |
double |
Angle that dictates how the feature appears on the map. |