Coupon
A coupon is a sample cut from a metal pipe to determine the extent of corrosion of the pipe. Coupons are generally taken as part of an exposed pipe inspection.
Subtypes: None
Associations: ExposedPipeInspection
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Comments |
text |
User and designer comments. |
|
CouponID |
text |
Identifier of associated coupon. |
|
EposedPipeInspectionObjectID |
long integer |
ObjectID of exposed pipe inspection. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
PercentOfGraph |
double |
Percent of graphitization. |
|
WallThickness |
text |
Thickness of pipe wall. |