Network Adapter Field Model Names
|
Model Name |
Object |
|---|---|
|
CYMDISTEXPORT |
Any attribute on a feature class that should be exported for use with the Electric Analysis engine provided by Cyme |
|
MSPKVARA |
KVAR on phase A |
|
MSPKVARB |
KVAR on phase B |
|
MSPKVARC |
KVAR on phase C |
|
MSPKWA |
Kilowatts on phase A |
|
MSPKWB |
Kilowatts on phase B |
|
MSPKWC |
Kilowatts on phase C |
|
MSPLOADCASE |
Denotes the name of the load case. This field is used to distinguish between multiple load values relating to the same feature. For example, you may store both winter peak and summer peak load values in the LoadCase table. You can do this by assigning a different load name to each record. "Winter Peak", and "Summer Peak", for example. |
|
MSPLOADFOREIGNKEY |
A unique ID for network features that have related load data. This field is used as a key between the LoadCase table and the network feature class that it is related to (typically TransformerBank or ServiceLocation), and it should be assigned to the key field in both the LoadCase table and the feature class. |
|
SYNERGEE_CONFIGURATION1 |
Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs. |
|
SYNERGEE_CONFIGURATION2 |
Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs. |
|
SYNERGEE_EQUIP1 |
Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs. |
|
SYNERGEE_EQUIP2 |
Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs. |
|
SYNERGEE_MANUFACTURER1 |
Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs. |
|
SYNERGEE_MANUFACTURER2 |
Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs. |
|
SYNERGEE_MECHANICALRESPONSE1 |
Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs. |
|
SYNERGEE_MECHANICALRESPONSE2 |
Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs. |
|
SYNERGEE_MODEL1 |
Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs. |
|
SYNERGEE_MODEL2 |
Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs. |
|
SYNERGEE_NEUTRALCONDUCTOR1 |
Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs. |
|
SYNERGEE_NEUTRALCONDUCTOR2 |
Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs. |
|
SYNERGEE_PHASECONDUCTOR1 |
Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs. |
|
SYNERGEE_PHASECONDUCTOR2 |
Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs. |