Capacitor Unit
Capacitors store electrical energy and release it back into the power system when required to reduce voltage drops. CapacitorUnit defines the following attributes:
Designer uses the DESIGNUNIT model name on this class to designate it as an electric device unit object class. The Designer Work Function Tool uses this model name to identify all electric device unit object classes.
Associations: CapacitorBank
Subtypes: None
Model Names: DESIGNUNIT
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
CapacitorBankObjectID |
long integer |
ObjectID of associated CapacitorBank. |
|
FluidType |
text |
Code indicating type of dielectric fluid (some contain polychlorinated biphenyls—PCBs) used in CapacitorUnit; domain values include Arachlor, Diachlor, Faradol, etc. |
|
kVAR |
long integer |
Code indicating CapacitorUnit size in kVAR; domain values include 100 kVAR, 150 kVAR, etc. |
|
Manufacturer |
text |
Code indicating manufacturer of CapacitorUnit. |