LeakSurveyArea
LeakSurveyArea is a general use polygon that describes areas of leak survey by due date.
Subtypes: None
Associations: None
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Comments |
text |
User or designer comments. |
|
DueDate |
date |
Date survey is due to be performed. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
InstallationDate |
date |
Date of installation. |
|
LastSurveyDate |
date |
Date of last survey. |
|
LeakSurveyDueDate |
date |
Due date of LeakSurvey. |
|
LeakSurveyFrequency |
text |
Code indicating frequency of leak survey; domain values include 3 Months, 12 Months, 36 Months, etc. |
|
SurveyAreaType |
text |
Type of survey area. |
|
TargetMonth |
text |
Target month that survey is to be performed. |