Induction Motor
InductionMotor is an electric transformer with a magnetic circuit separated by an air gap into two movable portions carrying the primary and secondary windings. Secondary currents are created by induction rather than being supplied by a dc exciter or other external power source. Types of induction motor are wound rotor and squirrel cage.
Induction motors have National Electric Manufacturers Association (NEMA) specifications.
Associations: ServicePoint
Subtypes: None
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
ConnectionConfiguration |
text |
Code indicating connection configuration of InductionMotor; domain values include Delta and Wye. |
|
Efficiency |
double |
Efficiency, expressed in percentage. |
|
GroundReactance |
double |
Ground reactance of InductionMotor in ohms. |
|
GroundResistance |
double |
Ground resistance of InductionMotor in ohms. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
LockedRotorMultiplier |
double |
Higher current required to start motor in percentage. |
|
LockedRotorPF |
double |
Power factor of locked rotor, expressed as less than one or as percentage. |
|
MotorStartLimit |
double |
Motor start limit. |
|
MotorStartLimitAmount |
double |
Motor start limit amount. |
|
NEMALockedRotorRatio |
double |
NEMA locked rotor kVA/HP ratio. |
|
NominalVoltage |
long integer |
Standard level of normal ratings for system voltage, expressed as line to line or line to neutral; domain values include 4.16 kV Grounded Y, 7.2 kV Grounded Y, etc. |
|
PhaseDesignation |
long integer |
Code indicating phases present; domain values include A, AB, AC, etc. |
|
PowerFactor |
double |
Power factor expressed as less than one or as percentage. |
|
RatedHP |
double |
Rated horsepower. |
|
ServicePointObjectID |
long integer |
ObjectID of ServicePoint. |
|
SoftStartReactance |
double |
Soft start reactance, X. |
|
SoftStartResistance |
double |
Soft start resistance, R. |
|
SoftStartTap |
double |
Soft start tap. |
|
SoftStartWinding |
double |
Soft start winding. |