International Data Model
|
Field Name |
Description |
|---|---|
|
CapacityToGround |
The capacitive reactance to neutral or earth of any line segment (ohms per map unit length). |
|
ConductorMaterial |
Material of which the conductor is made. |
|
ConductorSize |
Size of the conductor. |
|
ConnectionOKIndicator |
Indicates whether a line segment is capable of and ready for connection to a load or other line segment. |
|
InsulationType |
Insulation type of conductor. |
|
InsulationVoltage |
Withstand voltage of the conductor's insulation (Volts). |
|
MaxContinousCurrent |
Continuous current rating of conductor (Amperes). |
|
NumberConductorPerPhase |
Number of conductors per phase. |
|
OuterDiameter |
Outer diameter of conductor. |
|
OutOfOrderIndicator |
Indicates whether a line segment is de-energized (for example, out of service for maintenance). |
|
RatedCurrent |
Continuous current rating of conductor, including any de-rating required for special conditions (Amperes). |
|
Reactance |
Positive sequence reactance of conductor (ohms per map unit length). |
|
Resistance |
Positive sequence resistance of conductor (ohms per map unit length). |