PressureMonitoringDevice
Pressure monitoring devices monitor the flow of gas through a pipe and include pressure recorders, pressure telemeters, and pressure charts. An electronic PressureMonitoringDevice can monitor the flow of gas remotely using Supervisory Control and Data Acquisition (SCADA) systems to collect data.
PressureMonitoringDevice inherits characteristics from the abstract class GasDevice.
Subtypes: None
Associations: None
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
CompanyPaidTelephone |
text |
Code indicating whether device is monitored remotely; domain values include Yes or No. |
|
Duration |
long integer |
Length of time PressureMonitoringDevice will be active. |
|
LocationDescription |
text |
Verbal description of location of the pressure monitoring device. |
|
Manufacturer |
text |
Code indicating manufacturer. |
|
Model |
text |
Model number specified by manufacturer. |
|
PermanentIndicator |
text |
Indicates whether PressureMonitoringDevice is permanent; domain values include Yes or No. |
|
PSIRating |
text |
Pressure rating in psi. |
|
RecordingMethod |
text |
Method of reading device. |
|
SCADA |
text |
Code indicating whether device is SCADA monitored; domain values are Yes or No. |
|
SerialNumber |
text |
Serial number of monitoring device. |
|
TelephoneNumber |
text |
Telephone number of associated remote monitoring system. |
|
TempRating |
text |
Temperature rating for pressure telemeter. |
|
UsageType |
text |
Use type of device. |