Electric Device
ElectricDevice is an abstract class represented as a simple junction feature because devices connect to the logical network from a single insertion point. In general, electric devices help ensure consistent service within the distribution network. Electric devices either provide protection, such as fuses or circuit breakers, or regulate electric current such as transformers and voltage regulators.
Associations: FacilityStructure, UndergroundStructure (does not apply to OpenPoint)
Subtypes: None
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Comments |
text |
User or designer comments. |
|
ConstructionStatus |
long integer |
This field contains a value from the Construction Status domain that indicates the current status of construction on the structure (e.g., proposed, existing, retired). |
|
ElectricTraceWeight |
long integer |
Used by Feeder Manager to determine device status and other information that affects circuit connectivity. Feeder Manager requires that the MMELECTRICTRACEWEIGHT model name be assigned to this field. |
|
FacilityID |
text |
Meaningful company-assigned unique identifier of ElectricDevice. |
|
FeederID |
text |
Feeder Manager identifier assigned to feeders and devices that participate in a specific distribution circuit. Feeder Manager uses the FEEDERID model name in this field. |
|
FeederID2 |
text |
Feeder Manager identifier assigned if device is supplied by second feeder. Feeder Manager uses the FEEDERID2 model name in this field. |
|
FeederInfo |
long integer |
Feeder Manager-assigned phase information describing the phase of the circuit that supplies a device. Feeder Manager uses the FEEDERINFO model name on this field. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
InstallationDate |
date |
Date ElectricDevice was installed. |
|
NominalVoltage |
long integer |
Code indicating system voltage for which ElectricDevice is rated; domain values include 7.2 kV Grounded Y, 24.9 kV Grounded Y, 2400 Delta, 14.4 kV, etc. TIP: The Nominal Voltage
attribute does not apply to the following subclasses of ElectricDevice:
|
|
OperatingVoltage |
long integer |
Code indicating standard level at which system is currently being operated; may vary above or below nominal voltage; domain values include 4.16 kV Grounded Y, 7.2 kV Grounded Y, 2400 V Delta. Feeder Manager and Electric Tracing use the OPERATINGVOLTAGE model name on this field. |
|
PhaseDesignation |
long integer |
Code indicating phases supplying a device; domain values include A, AB, AC, etc. Feeder Manager and Electric Tracing require the PHASEDESIGNATION model name on this field. IMPORTANT: The PhaseDesignation attribute does not apply to the following subclasses:
Ground or FaultLimiter.
|
|
Subtype |
long integer |
Code indicating subtype. |
|
SymbolRotation |
double |
Angle of rotation indicating how a feature appears on the map. Uses the SYMBOLROTATION model name. The ArcFM Manual Angle Setter edit task, ArcFM Auto Angle Setter, Directional Auto Angle Setter, and Endpoint Auto Angle Setter autoupdaters use this field to rotate point features. |
|
WorkOrderID |
text |
Identifier of work order of ElectricDevice. |
|
ParentCircuitSourceID (optional) |
long integer |
This field contains a value that identifies the parent circuit source to the electric device. This field is required by Extended Feeder Manager. |
|
CircuitSourceID (optional) |
long integer |
This field contains the CircuitSourceID value for the electric device. This field is required by Extended Feeder Manager. |
|
SubSource (optional) |
short integer |
This contains a boolean value that indicates whether the device is considered a subsource. The Yes/No domain is assigned to this field. This field is required by Extended Feeder Manager. |