XML
The XML folder contains .dtd and .xsd files that verify the XML imported and exported by ArcFM. These files are found in the Program Files\Miner and Miner\ArcFM Solution\Bin\XML folder of the ArcFM Solution installation directory.
|
File Name |
Description |
Used by Tools: |
|---|---|---|
|
CU.dtd |
Validates the structure of CUs and GUs upon import. |
Designer |
|
CymdistImport.dtd |
Validates the XML exported from the geodatabase to ensure it is the proper structure before passing it to the CYMDIST API. |
Network Adapter |
|
DatabaseConnections.xml |
Stores connection information for ArcFM Viewer for ArcGIS Engine. Access this information using the ArcFM Engine Administrator. |
ArcFM Engine Administrator |
|
DatabaseProperties.dtd |
Validates the XML used by the Import/Export tool when importing or exporting database properties. |
XML Import/Export Tool |
|
Design.dtd |
Validates the structure of the design. |
Designer |
|
DesignOptimizationLayerSymbology.xml |
A sample file of Design Optimization symbology layers in XML format. |
Designer |
|
domains.dtd |
Validates the XML used by the Import/Export tool when importing or exporting domain information. |
XML Import/Export Tool |
|
FeatureClass.dtd |
Validates the XML used by the Import/Export tool when importing or exporting feature class information. |
XML Import/Export Tool |
|
FimObject.dtd |
Validates the XML used by the Import/Export tool when importing or exporting ArcFM properties information. |
XML Import/Export Tool |
|
GeometricNetwork.dtd |
Validates the XML used by the Import/Export tool when importing or exporting geometric network information. |
XML Import/Export Tool |
|
GraphicsFavorites.dtd |
Validates the XML used to import graphic favorites. |
Graphics Tab |
|
GxXML.dtd |
This .dtd wraps several other .dtds: Featureclass.dtd, Snapping.dtd, ModelNames.dtd, Domains.dtd, ObjectInfo.dtd, RelationshipClass.dtd, GeometricNetwork.dtd, and DatabaseProperties.dtd. |
XML Import/Export Tool |
|
Miner.layout.xsd |
Validates the XML used by the Custom Layout File. |
ArcFM Viewer for ArcGIS Engine |
|
MinervilleCymdistEquipment.xml |
Contains substation, generator, and motor equipment for the Minerville sample data. This equipment must be imported into CYMDIST before feeders can be exported from the Minerville sample data. |
Network Adapter |
|
modelnames.dtd |
Validates the XML used by the Import/Export tool when importing or exporting model name information. |
XML Import/Export Tool |
|
MspDefaults.xml |
Contains the default values for the MultiSpeak export for null fields. |
|
|
mspGeometry.xsd |
Contains definitions from the GML standard. This file is from the MultiSpeak consortium. |
Network Adapter |
|
Multispeak.xsd |
Defines features and attributes in the MultiSpeak specification. This file is from the MultiSpeak consortium. |
Network Adapter |
|
MultispeakRealTime.xsd |
Defines the message header information. It is used to validate MultiSpeak XML and references MultiSpeak.xsd and mspGeometry.xsd. This file is from the MultiSpeak consortium. |
Network Adapter |
|
NetworkAdapterGML.dtd |
Contains definitions for geometry in GML format. |
Network Adapter |
|
NetworkAdapterNetwork.dtd |
Validates the XML exported from the geodatabase to ensure it is the proper structure before passing it to the Vendor API. |
Network Adapter |
|
NetworkAdapterNetworkSample.xml |
The file provides sample XML that has been exported from a geodatabase and is ready to be passed to the Vendor API. |
Network Adapter |
|
NetworkAdapterResults.dtd |
Validates the XML used to import analysis results to the Analysis API. |
Network Adapter |
|
NetworkAdapterResultsSample.xml |
This file provides sample analysis results in XML format. |
Network Adapter |
|
NetworkAdapterTestCase.dtd |
Used for load cases. |
Network Adapter |
|
NetworkAdapterTestCaseSample.xml |
This file provides a sample load case in XML format. |
Network Adapter |
|
ObjectInfo.dtd |
Validates the XML used by the Import/Export tool when importing or exporting class extenion type and geo-object information. |
XML Import/Export Tool |
|
PxUsers.dtd |
Validates the XML used by the Process Framework Administration Tool when importing or exporting user information on the Import/Export tab. |
Process Framework Administration tool |
|
PxWorkflow.dtd |
Validates the XML used by the Process Framework Administration Tool when importing or exporting a Process Framework workflow on the Import/Export tab. |
Process Framework Administration tool (Designer/Workflow Manager only) |
|
PxXML.dtd |
This .dtd wraps two .dtds: PxWorkflow.dtd and WorkflowManagerCU.dtd. |
Process Framework Import/Export tool |
|
QAQC.dtd |
Validates the XML used by the QA/QC tool when the user elects to Write to File or Write All to File. |
QA/QC |
|
RelationshipClass.dtd |
Validates the XML used by the Import/Export tool when importing or exporting relationship class information. |
XML Import/Export Tool |
|
Sample.ArcFMViewer.exe.layout |
This is a sample copy of the custom laytout file used to distribute user interface customizations to ArcFM Viewer for ArcGIS Engine. |
ArcFM Viewer for ArcGIS Engine |
|
snapping.dtd |
Validates the XML used by the Import/Export tool when importing or exporting snapping information. |
XML Import/Export Tool |
|
WorkflowManagerCU.dtd |
Validates the XML used by the Process Framework Administration Tool when importing or exporting Compatible Units on the Import/Export tab. |
Process Framework Administration tool (Designer/Workflow Manager only) |