Maximum Allowable Pulling Tension with a Basket Weave Grip

The equations below calculate the maximum pulling tension if a basket-weave grip is used.
|
PILC Cable: (3/C Cables) |
ALS = p t (d - t) Tmax = 2000 x ALS |
|
Where: |
ALS = Area of lead sheath (in) Tmax = Maximum pulling tension (lb) t = Thickness of lead sheath (in) d = Outside diameter of lead sheath (in) |
|
Solid Dielectric Cables: |
Tmax = 2000 lb (600V, each) Tmax = 4000 lb (Primary, each) -- OR -- Tmax from the Maximum Pulling Tension Using Pulling Eye table. Compare; choose the lower Tmax |
Tension on a Single Cable
On a single cable pull, the basket-weave grip grips the entire circumference of the cable equally and transfers the force to the center of the cable. The maximim tension can be exerted on one cable.
Tension on Multiple Cables
On multiple cable pulls (more than one cable in a single grip) the entire grip does not tighten over all the cable as effectively as it does on a single cable. Therefore, there is an unequal distribution of the force on the cables. The equations for determining the maximum pulling tension for multiple cable pulls are:
Tension Distributed on Cables
|
If multiple cables pulls are: |
Follow table number: |
|---|---|
|
Same size, parallel lay (not triplex or quadruplex) |
1 |
|
Different sizes caused by including a separate neutral of a smaller size than the phase conductor |
2 |
|
Triplex or quadruplex |
3 |
Tension on Same Size Cables, Parallel Lay
|
Number of Cables |
Equation |
|---|---|
|
2 |
TTmax = Tmax x 1.5 |
|
3 |
TTmax = Tmax x 2.0 |
|
4 |
TTmax = Tmax x 3.0 |
|
Where: |
TTmax = Total maximum pulling tension Tmax = Maximum pulling tension/phase conductor |
Tension on Multiple Cables with Separate Neutrals
|
If: |
And: |
Then Use Equation: |
|---|---|---|
|
In a three cable pull where the neutral is the third cable |
The neutral is the same size or one stock size less than the phase conductor |
TTmax = Tmax x 2.0 |
|
The neutral is more than one stock size less than the phase conductor or bare |
TTmax = Tmax x 1.5 |
|
|
In a four cable pull where the neutral is the fourth cable |
The neutral is the same size or one stock size less than the phase conductor |
TTmax = Tmax x 3.0 |
|
The neutral is more than one stock size less than the phase conductor or bare |
TTmax = Tmax x 2.0 |
Tension on Triplex and Quadruplex Cables
|
Number of Cables |
Equation |
|---|---|
|
Triplex |
TTmax = (Tmax x 2.0) + NTmax |
|
Quadruplex |
TTmax = Tmax x 3.0) + NTmax |
|
Where: |
TTmax = Total maximum pulling tension Tmax = Maximum pulling tension/phase conductor NTmax = Maximum pulling tension/neutral conductor |