Strainer
Like a scrubber, this device is used to remove or “strain” foreign materials from natural gas (e.g., dirt, dust).
Subtypes: None
Associations: None
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Comments |
text |
User or designer comments. |
|
ConnectionDiameter |
text |
Size of connection. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
DesignPressureEntered |
double |
System pressure, in any unit of measure. |
|
DesignPressureStandard |
double |
Derived field displaying calculated standard system pressure. |
|
DesignPressureUnitOfMeasure |
text |
System pressure standard unit of measure; domain values include psi, iwc, etc. |
|
MaxDifferentialPressure |
double |
Maximum differential pressure rating across strainer. |
|
Owner |
text |
Owner of associated facility. |
|
PropertyUnitCode |
text |
Value assigned to assets to track and classify Property Records. |