AbandonedRemovedGasDevice
The AbandonedRemovedGasDevice feature represents gas devices that have been removed. It may also contain selected attributes of any gas device, depending on configuration.
Subtypes: None
Associations: None
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Comments |
text |
User or designer comments. |
|
DeviceType |
text |
Code indicating type of device. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
Manufacturer |
text |
Code indicating manufacturer. The AT_MANUFACATURER model name is used on this field to configure abandon for gas. |
|
Material |
text |
Code indicating material of GasDevice. The AT_MATERIAL model name is used on this field to configure abandon for gas. |
|
Model |
text |
Model number specified by manufacturer. The AT_MODEL model name is used on this field to configure abandon for gas. |
|
PropertyUnitCode |
text |
Value assigned to assets to track and classify property records. |
|
RetiredDate |
date |
The date the device was identified as abandoned. |
|
ValveDiameter |
text |
Diameter of GasValve. The AT_VALVESIZE model name is used on this field to configure abandon for gas. |
|
ValveType |
text |
Code indicating type of GasValve. The AT_VALVETYPE model name is used on this field to configure abandon for gas. |