Designer Field Model Names
|
Model Name |
Attribute |
|---|---|
|
DESIGNID |
DesignID attribute in all Feature Classes |
|
WORKFLOWSTATUS |
WorkFlowStatus attribute in all Feature Classes |
|
WORKFUNCTION |
WorkFunction attribute in all Feature Classes |
|
WORKLOCATIONID |
WorkLocationID attribute in all Feature Classes |
|
WORKREQUESTID |
WorkRequestID attribute in all Feature Classes |
|
Designer Non-Creatable Features |
|
|
Model Name |
Object |
|
DESIGN |
The Design Feature class in the Designer Dataset; prevents this feature class from displaying in the CU tab. |
|
WORKLOCATION |
The WorkLocation Feature class in the Designer Dataset; prevents this feature class from displaying in the CU tab. |
|
WORKREQUEST |
The WorkRequest Feature class in the Designer Dataset; prevents this feature class from displaying in the CU tab. |