Lifecycle History
LifecycleHistory is an abstract object provided so that administrators can relate information about the history of particular devices or equipment. This information is related to devices that have a spatial reference but is itself nonspatial. Define specific LifecycleHistory objects on an as-needed basis. As a new LifecycleHistory object is defined, you should also define any necessary relationships.
Subtypes: None
Associations: To be defined by user
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Comments |
text |
User or designer comments. |
|
FacilityID |
text |
Meaningful company-assigned unique identifier. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
WorkFunction |
text |
Code indicating life cycle phase; domain values include Install, Remove, Replace, Transfer, Retire, and Abandon. |
|
WorkOrderID |
text |
Utility identifier of work order. |