Electric Complex Edge
ElectricComplexEdge contains the common attributes of primary, secondary, overhead, and underground conductors. ElectricComplexEdge is an abstract class that includes subclasses such as busbars and communication cable. These are represented as complex edge features because multiple devices can be connected along their edge. Circuits are modeled with options for feeder identifiers to support automated switching and tracing functions.
SCADA applications in distribution systems are increasing in deregulated environments. Automated switching of feeder circuits involves supervisory control to support operator control of equipment. Data acquisition gathers telemetered data from a variety of sources to increase reliability and operator productivity.
Associations: None
Subtypes: None
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Comments |
text |
User or designer comments. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
LengthSource |
text |
Code indicating source of length measurement; domain values include Field Measurement and Mapping System. |
|
MeasuredLength |
long integer |
Length of ElectricComplexEdge. |
|
Subtype |
long integer |
Code indicating subtype of ElectricComplexEdge. |
|
WorkOrderID |
text |
Utility identifier of work order. |
|
Optional Fields |
||
|
ParentCircuitSourceID |
long integer |
This field contains a value that identifies the parent circuit source to the electric device. This field is required by Extended Feeder Manager. |