Customer Connection
CustomerConnection contains information about the service provided to the customer.
Associations: ServiceAddress
Subtypes: None
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Address |
text |
Customer address. |
|
Alternate[X,Y,Z] |
double |
Stores the X, Y, and Z values from a GPS device. |
|
AlternateSource |
text |
This field contains a value from the Feature Source domain that indicates an alternate source for the structure. |
|
ConnectionType |
text |
Type of connection. |
|
PhaseDesignation |
long integer |
Code indicating phases present; domain values include A, AB, AC, etc. Feeder Manager requires the PHASEDESIGNATION model name on this field for both ServicePoints and PrimaryMeters. |
|
ServiceCurrentRating |
short integer |
Code indicating maximum rating of service delivered to CustomerConnection; domain values include 100 amps, 600 amps, etc. |
International Data Model
In addition to the attributes listed above, the following attribute is used by the international electric data model.
|
Field Name |
Description |
|---|---|
|
CIS_ID |
ID of customer as known to a Customer Information System (CIS). |