Recloser Unit
Reclosers trip open a circuit for a short time to clear temporary fault and reclose after a predetermined time. The time-current characteristic, usually expressed in a curve, is based on temperature and fuse tolerances and is used to coordinate recloser operations.
Designer uses the DESIGNUNIT model name on this class to designate it as an electric device unit object class. The Designer Work Function Tool uses this model name to identify all electric device unit object classes.
Associations: Recloser
Subtypes: None
Model Names: DESIGNUNIT
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Manufacturer |
text |
Code indicating manufacturer. |
|
RecloserObjectID |
long integer |
ObjectID of associated Recloser. |
|
ReversePowerAccessory |
text |
Code indicating whether recloser has Reverse Power Accessory; values are Yes or No. |