CathodicProtectionDevice
CathodicProtectionDevice is an abstract class. Cathodic protection systems prevent corrosion in underground metal structures such as steel pipes, fittings, and valves. Metal structures corrode because stray electric current flows from the relatively “anodic” structure to “cathodic” soil. To prevent this, cathodic protection systems provide a source of current to make the metal cathodic, causing the current to flow from the source, through the soil (which acts as an electrolyte), and to the pipe thus preventing corrosion. Insulation is also used to reduce the amount of corrosion on pipes.
Cathodic protection systems consist of a source of direct current (often a rectifier), anodes, and wire. Current flows from the source through the ground bed containing anodes, through the soil to the pipe, and back to the rectifier. Electrons flow away from the ground bed to the pipe. This causes the anodes to deteriorate over time, but the pipe is protected.
CPTestPoint, CPAnode, CPRectifier, and CPBondJunction derive attributes from the CathodicProtectionDevice abstract class.
Subtypes: None
Associations: CPSystem
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Comments |
text |
User or designer comments. |
|
GasTraceWeight |
long integer |
Information used for tracing analysis; stored in a bitgate. To support Gas Tracing and Feeder Manager, the model name GASTRACEWEIGHT is required for every feature class belonging to ArcFM gas networks. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
InServiceDate |
date |
Date pipe set in service. |
|
InstallationDate |
date |
Date of installation. |
|
LocationDescription |
text |
Verbal description of location of device; examples include Casings, Insulated Fittings, and Foreign Pipelines. |
|
OperatingStatus |
text |
Code indicating functional status of device; examples include Active, Designed, and Proposed Retire. |
|
PropertyUnitCode |
text |
Value assigned to assets to track and classify Property Records. |
|
SubType |
long integer |
Code indicating type of Cathodic Protection Device;examples include Anode, Rectifier, and Bond Junction. |
|
SymbolRotation |
double |
Angle that dictates how the feature appears on the map. |
|
WorkOrderID |
text |
Utility-defined identifier of work order. |