CPBondWire
Bond wire connects two nonadjacent sections of pipe to maintain the pipe in a “cathodic” state. CPBondWire is considered a simple edge feature because it is connected to other devices only at its ends and is used to perform traces to test the cathodic protection system.
You may omit specific feature classes from gas traces. To do this, assign the GASNONTRACABLE model name to the CPBondWire feature class. The GASNETWORKEDGE model name is used to configure gas tracing in ArcFM Viewer for ArcGIS Engine. Assign to all Gas Network Edge feature classes that participate in gas tracing
Subtypes: None
Associations: CPBondJunction, CPSystem
Model Names: GASNETWORKEDGE, GASNONTRACABLE
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Color |
text |
Color assigned to CPSection; domain values include Aqua, Forest, and Pink. |
|
Comments |
text |
Comments of user or designer. |
|
CPSystemObjectID |
long integer |
Object ID of associated system. |
|
Depth |
double |
Depth of CPBondWire. |
|
GasTraceWeight |
long integer |
Information used for tracing analysis; stored in a bitgate. Gas tracing uses the GASTRACEWEIGHT model name on this field. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
InServiceDate |
date |
Date bond wire was set in service. |
|
InstallationDate |
date |
Date bond wire was installed. |
|
LengthSource |
text |
Source of length measurement; domain values are Mapping System and Field Measurement. |
|
LocationDescription |
text |
Verbal description of location of bond wire. |
|
Material |
text |
Code indicating material of wire. |
|
MeasuredLength |
double |
Field-measured length of CPBondWire, ranging from 1 to 1,000,000,000. Gas tracing uses the MEASUREDLENGTH model name on this field. |
|
OperatingStatus |
text |
Code indicating functional status of CPBondWire; domain values include Active, Designed, and Proposed Retire. |
|
PropertyUnitCode |
text |
Value assigned to assets to track and classify. |
|
WireDiameter |
text |
Diameter of CPBondWire. |
|
WireSize |
text |
Size of CPBondWire. |
|
WorkOrderID |
text |
Utility-defined identifier of work order. |