Capacitor Control
Capacitors maintain or increase the voltage of distribution conductors and reduce voltage drops in the system. Subtypes include CurrentLevel, KVARLevel, TempLevel, Time, and VoltageLevel.
Associations: CapacitorBank, SeriesCapacitor
Subtypes: Current Level, KVAR Level, Temp Level, Time, Voltage Level. The use of subtypes is optional. The Subtype attribute can be removed if subtypes aren't used in the model.
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
DeactivateSaturday |
text |
Code indicating whether capacitor control deactivates on Saturday; domain values are Yes or No. |
|
DeactivateSunday |
text |
Code indicating whether capacitor control deactivates on Sunday; domain values are Yes or No. |
|
OnSetting |
long integer |
Indicates when capacitor bank is turned on. |
|
OffSetting |
long integer |
Indicates when capacitor bank is turned off. |
|
PFCorrectingEquipObjectID |
long integer |
ObjectID of associated PFCorrectingEquipment. |
|
Phase |
text |
Code describing phases attached to capacitor bank; domain values include A, AB, AC, etc. |
|
SCADAControlID |
text |
ID of SCADA control, if present. |
|
SCADAMonitorID |
text |
ID of SCADA monitor, if present. |