Electric Field Model Names
|
Model Name |
Object |
|---|---|
|
ACTUALDUCTSIZE |
ActualDuctSize attribute in DuctDefinition object (optional) |
|
AT_<Field Name> |
Any attribute of a source feature class that should be transferred to the abandoned (destination) feature class; must also exist on the corresponding field of the destination feature/object class |
|
CLASS |
Assign to attribute that represents class of structure; used for structural analysis |
|
CIRCUITSOURCEGLOBALID |
Assign to the GlobalID field in CircuitSourceID tables. This field and field model name enable Extended Feeder Manager to use Global IDs. |
|
CIRCUITSOURCEGUID |
Assign to the GUID field added to any table except the CircuitSourceID table. This field and field model name enable Extended Feeder Manager to use GUIIDs. IMPORTANT: Do NOT assign this to the CircuitSourceID
table.
|
|
CIRCUITSOURCEID |
Assign to the CircuitSourceID field. This field and field model name are used by Feeder Manager to support multi-tiered networks. |
|
CONDUCTORMATERIAL |
Assign to attribute of ConductorInfo or overhead conductor feature class that represents material of conductor; used for structural analysis |
|
CONDUCTORSIZE |
Assign to attribute of ConductorInfo or overhead conductor feature class that represents size of conductor; used for structural analysis |
|
DEVICETYPE |
Indicates the type of device. Assigned to the DeviceType field on the MMENG_DEVICEWEIGHT field for Structural Analysis (Designer only). |
|
DIAMETER |
The attribute on any overhead support structure feature class that represents the diameter of the structure; used for structural analysis |
|
DUCTAVAILABILITY |
Available attribute in DuctDefinition object |
|
DUCTBANKCONFIGURATION |
DuctBankConfiguration attribute in conduit feature class with ULS model name |
|
DUCTBANKHEIGHT |
Height attribute in DuctDefinition object (optional) |
|
DUCTBANKWIDTH |
Width attribute in DuctDefinition object (optional) |
|
DUCTID |
DuctID attribute in DuctDefinition object (optional) |
|
DUCTMATERIAL |
Material attribute in DuctDefinition object |
|
DUCTNAME |
Name attribute on the Duct feature class |
|
DUCTOCCUPIED |
Occupied field on the Duct feature class |
|
DUCTSIZE |
DuctSize attribute in DuctDefinition object |
|
FACILITYDIAGRAM |
FacilityDiagram field on the UndergroundStructure feature class |
|
FACILITYID |
Assign to FacilityID field of Transformer feature class; used by Secondary Circuit Analysis |
|
FDRMGRGANGOPERATED |
Indicates whether a device is gang operated. |
|
FDRMGRNONTRACEABLE |
The attribute on any feature class that indicates whether a feature should be traced by Feeder Manager. For a detailed explanation of FDRMGRNONTRACEABLE, view the appendix help topic: Appendix > Bitgate Fields > Electric Tracing - Edges. |
|
FEEDERID |
The FeederID field in any network listed as part of a feeder; also the FeederID field in the CircuitSource object |
|
FEEDERID2 |
The FeederID2 field in any network listed as part of a feeder |
|
FEEDERINFO |
The FeederInfo field in any network feature listed as part of a feeder |
|
FEEDERLEVEL |
Assign to the FeederLevel field. This field and field model name are used by Feeder Manager to support multi-tiered networks. |
|
FEEDERNAME |
The FeederName in the CircuitSource object. |
|
FEEDERSOURCEINFO |
The FeederSourceInfo field in the CircuitSource object |
|
GROUNDREACTANCE |
Ground reactance field of Transformer |
|
GR0UNDRESISTANCE |
Ground resistance field of Transformer |
|
GUYCOUNT |
Assign to attribute on AnchorGuy feature class that represents the number of guys in the system; used for structural analysis |
|
HASSUBDUCTS |
HasSubducts field on the Duct feature class |
|
HEIGHT |
Assign to attribute on AnchorGuy feature class that represents the height of the structure; used for structural analysis |
|
HIGHSIDECONFIGURATION |
Assign to HighSideConfiguration field of Transformer |
|
HIGHSIDEGROUNDREACTANCE |
Assign to HighSideGroundReactance field of Transformer |
|
HIGHSIDEGROUNDRESISTANCE |
Assign to HighSideGroundResistance field of Transformer |
|
INSULATIONTYPE |
Assign to insulation type field |
|
JOINTATTACHMENTOWNER |
Assign to the Owner field of the JointUseAttachment table |
|
LASSOTEXT |
The LassoText field in the Lasso feature class (ULS/contents relate tool) |
|
LASSOTEXTFIELD |
Assign to field that is source for a different label than label in the contents list of cross section annotation feature for a conductor or cable feature class contained in a conduit system |
|
LEADLENGTH |
Assign to lead length field |
|
LOWSIDECONFIGURATION |
Assign to LowSideConfiguration field of Transformer |
|
LOWSIDEGROUNDREACTANCE |
Assign to LowSideGroundReactance field of Transformer |
|
LOWSIDEGROUNDRESISTANCE |
Assign to LowSideGroundResistance field of Transformer |
|
LOWSIDEVOLTAGE |
Assign to LowSideVoltage field of Transformer |
|
MANUFACTURERMODEL |
Assign to the Manufacturer Model field in the MMENG_DEVICEWEIGHT table for Structural Analysis. Designer only. |
|
MATERIAL |
Assign to attribute on overhead support structure feature class that represents the material; used for structural analysis |
|
MMELECTRICTRACEWEIGHT |
Assign to electric trace weight field of features participating in Feeder Manager and electric trace tasks |
|
MMSECCKTAMPACITY |
Assign to Ampacity field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis |
|
MMSECCKTCODE |
Assign to Code field of MMENG_TRANSFORMER and MMENG_CONDUCTOR_ELEC tables; used for secondary circuit analysis |
|
MMSECCKTCOST |
Assign to Cost field of MMENG_TRANSFORMER and MMENG_CONDUCTOR_ELEC tables; used for secondary circuit analysis |
|
MMSECCKTCUCODE |
Assign to CUCode field of MMENG_TRANSFORMER and MMENG_CONDUCTOR_ELEC tables; used for secondary circuit analysis |
|
MMSECCKTDESCRIPTION |
Assign to Description field of MMENG_TRANSFORMER and MMENG_CONDUCTOR_ELEC tables; used for secondary circuit analysis |
|
MMSECCKTINSULATION |
Assign to Insulation field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis |
|
MMSECCKTMATERIAL |
Assign to Material field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis |
|
MMSECCKTR_PER1000UNITSLENGTH |
Assign to R_Per1000_Units_Length field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis |
|
MMSECCKTR0_PER1000UNITSLENGTH |
Assign to R0_Per1000_Units_Length field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis |
|
MMSECCKTSIZE |
Assign to CondSize field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis |
|
MMSECCKTTRANSFORMERFULLLOADLOSSMAX |
Assign to FULL_LOAD_LOSS_MAX field of MMENG_TRANSFORMER table; used for secondary circuit analysis |
|
MMSECCKTTRANSFORMERNOLOADLOSSMIN |
Assign to FULL_LOAD_LOSS_MIN field of MMENG_TRANSFORMER table; used for secondary circuit analysis |
|
MMSECCKTTRANSFORMERKVA |
Assign to kVA field of MMENG_TRANSFORMER table; used for secondary circuit analysis |
|
MMSECCKTTRANSFORMERMAXXTOR |
Assign to X_TO_R_MAX field of MMENG_TRANSFORMER table; used for secondary circuit analysis |
|
MMSECCKTTRANSFORMERMAXZ |
Assign to Percent_Z_MAX field of MMENG_TRANSFORMER table; used for secondary circuit analysis |
|
MMSECCKTTRANSFORMERMINXTOR |
Assign to X_TO_R_MIN field of MMENG_TRANSFORMER table; used for secondary circuit analysis |
|
MMSECCKTTRANSFORMERMINZ |
Assign to Percent_Z_MIN field of MMENG_TRANSFORMER table; used for secondary circuit analysis |
|
MMSECCKTTRANSFORMERNOLOADLOSSMAX |
Assign to NOLOAD_LOSS_MAX field of MMENG_TRANSFORMER table; used for secondary circuit analysis |
|
MMSECCKTTRANSFORMERNOLOADLOSSMIN |
Assign to NOLOAD_LOSS_MIN field of MMENG_TRANSFORMER table; used for secondary circuit analysis |
|
MMSECCKTTRANSFORMERPHASES |
Assign to Phasing field of MMENG_TRANSFORMER table; used for secondary circuit analysis |
|
MMSECCKTUNDERGROUND |
Assign to Underground field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis |
|
MMSECCKTX_PER1000UNITSLENGTH |
Assign to X_Per1000_Units_Length field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis |
|
MMSECCKTX0_PER1000UNITSLENGTH |
Assign to X0_Per1000_Units_Length field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis |
|
NEUTRALMATERIAL |
Assign to attribute on overhead support structure feature class that represents the material of neutral cable; used for structural analysis |
|
NEUTRALSIZE |
Assign to attribute on overhead support structure feature class that represents the size of the neutral cable; used for structural analysis |
|
NOMINALVOLTAGE |
Used by the ArcFM Inherit Nominal Voltage autoupdater. Assign to the Nominal Voltage field on the Primary Conductor and Transformer feature classes. |
|
NORMALPOSITION_A |
The attribute on all switchable feature classes (e.g., fuse, switch) that indicates the position (open or closed) of phase A |
|
NORMALPOSITION_B |
The attribute on all switchable feature classes (e.g., fuse, switch) that indicates the position (open or closed) of phase B |
|
NORMALPOSITION_C |
The attribute on all switchable feature classes (e.g., fuse, switch) that indicates the position (open or closed) of phase C |
|
NUMBERCONDUCTORSPERPHASE |
Assign to attribute on ConductorInfo or overhead conductor feature class that represents the number of conductors present for each phase; used for structural analysis |
|
OPERATINGVOLTAGE |
The attribute on any conductor feature class or bus bar feature class that indicates the operating voltage of the feature |
|
PARENTCIRCUITSOURCEGUID |
Assign to the GUID field added to any table, including any CircuitSourceID table, that had the field model name PARENTCIRCUITSOURCEID assigned to a field. Used by Extended Feeder Manager to support the use of GlobalIDs. |
|
PARENTCIRCUITSOURCEID |
Assign to the ParentCircuitSourceID field. This field and field model name are used by Feeder Manager to support multi-tiered networks. |
|
PHASEDESIGNATION |
The attribute on any Conduit System member that indicates the phase of the feature (to support Conduit System Management); the attribute on any transformer feature class or load point feature class (e.g., PrimaryMeter) that indicates the phase of the feature (to support Feeder Manager); the attribute on any conductor that indicates the phase of the conductor (to support the Auto Phase Assign autoupdater) |
|
RATEDKVA |
The RatedKVA field in the DistributionTransformer feature class and the TransformerUnit object |
|
RATING |
Assign to the Rating field in the MMENG_DEVICEWEIGHT table for Structural Analysis. Designer only. |
|
RELATEDFEATURECLASSNAME |
Assign to the RelatedFeatureClassName field. This field and field model name are used by Feeder Manager to support multi-tiered networks. |
|
RELATEDOBJECTID |
Assign to the RelatedObjectID field. This field and field model name are used by Feeder Manager to support multi-tiered networks. |
|
SERIALNUMBER |
Assign to the Serial Number field in the MMENG_DEVICEWEIGHT table for Structural Analysis. Designer only. |
|
SERVICECURRENTRATING |
Assign to service current rating field; used by secondary circuit analysis |
|
SUBSOURCE |
Assign to the SubSource field. This field and field model name are used by Feeder Manager to support multi-tiered networks. |
|
SUBSTATIONID |
The SubstationID field in the CircuitSource object |
|
SUBTYPECD |
The field on the Duct Definition object class that indicates the subtypes defined |
|
ULSTEXTFIELD |
In a ULSMember, designates field used for display in Cross Section contents list (optional) |
|
USAGETYPE |
The attribute on any overhead support structure feature class that represents the type of use of the structure; used for structural analysis |
|
WIRESIZE |
Assign to attribute on AnchorGuy that represents the guy wire size; used for structural analysis |
|
WIRESTRENGTH |
Assign to attribute on AnchorGuy that represents the guy wire strength classification; used for structural analysis |