SqueezeOff
A SqueezeOff represents a section of pinched pipe.
Gas tracing requires the SQUEEZEOFF class model name and is used to determine whether pinching the pipes at selected locations will isolate an area.
Subtypes: None
Associations: Meter
Model Names: SQUEEZEOFF
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Comments |
text |
User or designer comments. |
|
GasTraceWeight |
long integer |
Information used for tracing analysis; stored in a bitgate. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
NormalPosition |
long integer |
Normal position of GasValve; domain values include Open and Closed. |
|
SymbolRotation |
double |
Angle that dictates how the feature appears on a map. |
|
Subtype |
Code indicating type of GasDevice, examples include Gas Lamp, Relief Valve, and Gas Station. |