Recloser Hydraulic Control
Hydraulic control is an integral part of single-phase reclosers. A trip coil in series with the line is used to sense overcurrent and trip open the recloser contacts. The contacts close after a preset interval.
Associations: None
Subtypes: None
Model Names:
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
CoilSize |
short integer |
Code indicating size of trip coil in amps; domain values include 25 amps, 50 amps, etc. |
|
RecloseInterval |
long integer |
Amount of time before reclosing between operations. |
|
ResetTime |
long integer |
Amount of time Recloser resets to beginning of operation sequence. |
|
TCC1Operations |
long integer |
Number of trips per curve for slow trip. |
|
TCC2Operations |
long integer |
Number of trips per curve for fast trip. |
|
TCC1Selection |
long integer |
Specific curve selected for slow trip. |
|
TCC2Selection |
long integer |
Specific curve selected for fast trip. |